B.3.8: Speeding Up Automatic Attribute Reports
Automatic attribute reports (configured as described in Appendix B.3.5) that are produced on changes in attribute values can be speeded up to occur with millisecond resolution. Normally, these reports can occur on a timescale of seconds, as they are dependent on the E_ZCL_CBET_TIMER (one second) ticks for sampling. However, they can be made to occur on a timescale of milliseconds by providing E_ZCL_CBET_TIMER_MS (one millisecond) ticks.
In order to do this, the following code must be included in the application:
sCallBackEvent.eEventType = E_ZCL_CBET_TIMER_MS;
vZCL_EventHandler(&sCallBackEvent);
Note that the E_ZCL_CBET_TIMER ticks still need to be generated, as they are used by UTC time and by the ZCL report manager to keep track of time.
Parent topic:Appendix B.3: Configuring attribute reporting