Functions
The following Appliance Events and Alerts cluster functions are provided:
eCLD_ApplianceEventsAndAlertsCreateApplianceEventsAndAlerts
teZCL_Status eCLD_ApplianceEventsAndAlertsCreateApplianceEventsAndAlerts(
tsZCL_ClusterInstance *psClusterInstance,
bool_t bIsServer,
tsZCL_ClusterDefinition *psClusterDefinition,
oid *pvEndPointSharedStructPtr,
uint8 *pu8AttributeControlBits,
tsCLD_ApplianceEventsAndAlertsCustomDataStructure
*psCustomDataStructure);
Description
This function creates an instance of the Appliance Events and Alerts cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance structure and can act as a server or a client, as specified.
The function should only be called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function creates an Appliance Events and Alerts cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions. For more details of creating cluster instances on custom endpoints, refer to Appendix D.
Note: This function must not be called for an endpoint on which a standard ZigBee device is used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function from those described in the ZigBee Devices User Guide*(JNUG3131)*.
When used, this function must be the first Appliance Events and Alerts cluster function called in the application, and must be called after the stack has been started and after the ZCL has been initialized.
The function requires an array to be declared for internal use, which contains one element (of type uint8) for each attribute of the cluster. The array length is automatically adjusted by the compiler using the following declaration:
uint8 au8ApplianceEventsAndAlertsAttributeControlBits
[(sizeof(asCLD_ApplianceEventsAndAlertsClusterAttributeDefinitions)
/ sizeof(tsZCL_AttributeDefinition))];
Parameters
Returns
Parent topic:Functions
eCLD_AEAAGetAlertsSend
teZCL_Status eCLD_AEAAGetAlertsSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber);
Description
This function can be used on an Appliance Events and Alerts cluster client to send a ‘Get Alerts’ message to a cluster server (appliance).
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the message. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameter
Returns
Parent topic:Functions
eCLD_AEAAGetAlertsResponseORAlertsNotificationSend
teZCL_Status eCLD_AEAAGetAlertsResponseORAlertsNotificationSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
teCLD_ApplianceEventsAndAlerts_CommandId eCommandId,
tsCLD_AEAA_GetAlertsResponseORAlertsNotificationPayload
*psPayload);
Description
This function can be used on an Appliance Events and Alerts cluster server to send a ‘Get Alerts Response’ message (in reply to a ‘Get Alerts’ message) or an unsolicited ‘Alerts Notification’ message to a cluster client.
The command to be sent must be specified as one of:
E_CLD_APPLIANCE_EVENTS_AND_ALERTS_CMD_GET_ALERTS
E_CLD_APPLIANCE_EVENTS_AND_ALERTS_CMD_ALERTS_NOTIFICATION
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the message. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
Returns
Parent topic:Functions
eCLD_AEAAAlertsNotificationSend
teZCL_Status eCLD_AEAAAlertsNotificationSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_AEAA_GetAlertsResponseORAlertsNotificationPayload
*psPayload);
Description
This function can be used on an Appliance Events and Alerts cluster server to send an unsolicited ‘Alerts Notification’ message to a cluster client. The function is an alternative to eCLD_AEAAGetAlertsResponseORAlertsNotificationSend().
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the message. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
Returns
Parent topic:Functions
eCLD_AEAAEventNotificationSend
teZCL_Status eCLD_AEAAEventNotificationSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_AEAA_EventNotificationPayload *psPayload);
Description
This function can be used on an Appliance Events and Alerts cluster server (appliance) to send an ‘Event Notification’ message to a cluster client, to indicate that an incident has occurred.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the message. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
Returns
Parent topic:Functions
Parent topic:Appliance Events and Alerts Cluster