eCLD_PollControlUpdate
teZCL_Status eCLD_PollControlUpdate(void);
Description
This function can be used on a cluster server to update the timing status for the following periodic activities:
polling of the parent for a data packet
‘check-ins’ with the client to check for a required change in the poll mode
The function should be called once per quarter-second and the application should provide a 250-ms timer to prompt these function calls.
Any poll or check-in that is due when this function is called are automatically performed by the cluster server.
Parameters
None
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
Parent topic:Server Functions