eCLD_PollControlUpdateSleepInterval
teZCL_Status eCLD_PollControlUpdateSleepInterval(
uint32 u32QuarterSecondsAsleep);
Description
This function can be used on a cluster server to provide the updated ticks back into PollControl cluster for the time the device was sleeping in terms of quarter second.
This function updates the Checkin period based on the ticks provided.
Parameters
u32QuarterSecondsAsleep: Number of Quarter seconds the device has slept for
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_CLUSTER_NOT_FOUND
Parent topic:Server Functions