eCLD_PPEnergyPhaseScheduleStateNotificationSend
teZCL_Status eCLD_PPEnergyPhasesScheduleStateNotificationSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_PP_EnergyPhasesSchedulePayload
*psPayload);
Description
This function can be used on the cluster server to send an Energy Phases Schedule State Notification to a cluster client, in order to inform the client of the energy phases that are in the schedule of a particular power profile. The function is used to send an unsolicited command.
On receiving the notification on the client, the event E_CLD_PP_CMD_ENERGY_PHASES_SCHEDULE_STATE_NOTIFICATION is generated, containing the sent power profile information in a tsCLD_PP_EnergyPhasesSchedulePayload structure (see Section 21.10.6).
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the message. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
u8SourceEndPointId: Number of local endpoint on which cluster server resides
u8DestinationEndPointId: Number of remote endpoint on which cluster client resides
psDestinationAddress: Pointer to a structure containing the destination address of the client node
psDestinationAddress: Pointer to a location to receive the Transaction Sequence Number (TSN) of the message
*psPayload: Pointer to structure containing the payload for the request (see Section 21.10.6), including the identifier of the relevant power profile and the associated schedule of energy phases
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
Parent topic:Server Functions