eCLD_PPGetOverallSchedulePriceSend
teZCL_Status eCLD_PPGetOverallSchedulePriceSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber);
Description
This function can be used on the cluster server to send a Get Overall Schedule Price Request to a cluster client, in order to obtain the overall cost of all the power profiles that are executed over the next 24 hours. Use of this function must be enabled in the cluster compile-time options, as described in Section 21.11.
The function is non-blocking and will return immediately. On successfully receiving a Get Overall Schedule Price Response from the client, an E_CLD_PP_CMD_GET_OVERALL_SCHEDULE_PRICE_RSP event is generated on the server, containing the required price information in a tsCLD_PP_GetOverallSchedulePriceRspPayload structure (see Section21.10.10). For full details of handling a Get Overall Schedule Price Request, refer to Section 21.5.6.2.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the message. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
u8SourceEndPointId: Number of local endpoint on which cluster server resides
u8DestinationEndPointId: Number of remote endpoint on which cluster client resides
psDestinationAddress: Pointer to a structure containing the destination address of the client node
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the message
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
Parent topic:Server Functions