eCLD_PPGetPowerProfilePriceSend
teZCL_Status eCLD_PPGetPowerProfilePriceSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_PP_PowerProfileReqPayload *psPayload);
Description
This function can be used on the cluster server to send a Get Power Profile Price Request to a cluster client, in order to request the cost of executing the schedule of a particular power profile. Use of this function must be enabled in the cluster compile-time options, as described in Section 21.11.
The function is non-blocking and will return immediately. On successfully receiving a Get Power Profile Price Response from the client, an E_CLD_PP_CMD_GET_POWER_PROFILE_PRICE_RSP event is generated on the server, containing the requested price information in a tsCLD_PP_GetPowerProfilePriceRspPayload structure (see Section21.10.9). For full details of handling a Get Power Profile Price Request, refer to Section 21.5.6.1.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the message. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
u8SourceEndPointId Number of local endpoint on which cluster server resides
u8DestinationEndPointId Number of remote endpoint on which cluster client resides
psDestinationAddress Pointer to a structure containing the destination address of the client node
pu8TransactionSequenceNumber Pointer to a location to receive the Transaction Sequence Number (TSN) of the message
psPayload Pointer to structure containing the payload for the request (see Section 21.10.5), including the identifier of the relevant power profile
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
Parent topic:Server Functions