eCLD_PPPowerProfileScheduleConstraintsNotificationSend
teZCL_Status eCLD_PPPowerProfileScheduleConstraintsNotificationSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_PP_PowerProfileScheduleConstraintsPayload
*psPayload);
Description
This function can be used on the cluster server to send a Power Profile Schedule Constraints Notification to a cluster client, in order to inform the client of the schedule restrictions on a particular power profile. The constraints are specified in a tsCLD_PP_PowerProfileScheduleConstraintsPayload structure (see Section 21.10.7). They can subsequently be used by the client in calculating the schedule for the energy phases of the power profile. The function is used to send an unsolicited command.
On receiving the notification on the client, the event E_CLD_PP_CMD_SCHEDULE_CONSTRAINTS_NOTIFICATION is generated, containing the sent power profile constraint information in a tsCLD_PP_PowerProfileScheduleConstraintsPayload structure.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the message. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
u8SourceEndPointId: Number of local endpoint on which cluster server resides
u8DestinationEndPointId : Number of remote endpoint on which cluster client resides
psDestinationAddress: Pointer to a structure containing the destination address of the client node
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the message
psPayload: Pointer to structure containing the payload for the request (see Section 21.10.7), including the identifier of the relevant power profile and the associated schedule constraints
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
Parent topic:Server Functions