eCLD_PPPowerProfileScheduleConstraintsReqSend
teZCL_Status eCLD_PPPowerProfileScheduleConstraintsReqSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_PP_PowerProfileReqPayload *psPayload);
Description
This function can be used on a cluster client to send a Power Profile Schedule Constraints Request to the cluster server, in order to obtain the schedule restrictions on a particular power profile on the server. The obtained constraints can subsequently be used in calculating a schedule of energy phases for the power profile (e.g. before calling eCLD_PPEnergyPhasesScheduleNotificationSend()).
The function is non-blocking and will return immediately. The server will send a response to this request and on receiving this response, an E_CLD_PP_CMD_GET_POWER_PROFILE_SCHEDULE_CONSTRAINTS_RSP event is generated on the client, containing the requested schedule constraints in a tsCLD_PP_PowerProfileScheduleConstraintsPayload structure (see Section 21.10.7).
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the message. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
u8SourceEndPointId: Number of local endpoint on which cluster client resides
u8DestinationEndPointId : Number of remote endpoint on which cluster server resides
psDestinationAddress: Pointer to a structure containing the destination address of the server node
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the message
psPayload: Pointer to structure containing the payload for the request (see Section 21.10.3), including the identifier of the relevant power profile
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
Parent topic:Client Functions