eCLD_PPRemovePowerProfileEntry
teZCL_Status eCLD_PPRemovePowerProfileEntry(
uint8 u8SourceEndPointId,
uint8 u8PowerProfileId);
Description
This function can be used on a cluster server to remove a power profile by deleting the relevant entry in the local power profile table.
Parameters
u8SourceEndPointId: Number of local endpoint on which cluster resides:
u8PowerProfileId : Identifier of power profile to be removed
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
Parent topic:Server Functions