eCLD_PPSchedule
teZCL_Status eCLD_PPSchedule(void);
Description
This function can be used on a cluster server to update the state of the currently active power profile and the timings required for scheduling. When called, the function automatically makes any required changes according to the scheduled energy phases for the power profile. If no change is scheduled, the function only updates timing information. If a change is required, it also updates the power profile state and the ID of the energy phase currently being executed.
The function should be called once per second to progress the active power profile schedule and the application should provide a 1-second timer to prompt these function calls.
Parameters
None
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_INVALID_VALUE
Parent topic:Server Functions