Requesting a schedule (by server)
The server application can request a schedule for a supported power profile from the client by calling the function eCLD_PPEnergyPhasesScheduleReqSend(), which sends an Energy Phases Schedule Request to the client.
The client can only return the requested schedule information if it stores this type of information for the power profile. If this is the case, an E_CLD_PP_CMD_ENERGY_PHASES_SCHEDULE_REQ event is generated on the client, with the bIsInfoAvailable field set to TRUE in the event structure tsCLD_PPCallBackMessage, and the client will send an Energy Phases Schedule Response back to the server. Otherwise, the client sends a ZCL default response with status NOT_FOUND.
On receiving an Energy Phases Schedule Response from the client, the event E_CLD_PP_CMD_ENERGY_PHASES_SCHEDULE_RSP is generated on the server, containing the requested schedule information in a tsCLD_PP_EnergyPhasesSchedulePayload structure (see Section 21.10.6). One or more of the following outcomes result:
If the attribute
bEnergyRemoteis set to FALSE on the server (no remote control of the device), the server simply rejects the received schedule.If the received schedule information contains an
u16MaxActivationDelayvalue of zero for an energy phase (see tsCLD_PP_EnergyPhaseInfo), this energy phase is rejected by the server although other valid energy phases are accepted. For each rejected energy phase, the server sends a ZCL default response with status NOT_AUTHORIZED to the client.If the received schedule information results in an update of the power profile schedule on the server, the server automatically sends an Energy Phases Schedule State Notification back to the client. On receiving this notification, an E_CLD_PP_CMD_ENERGY_PHASES_SCHEDULE_STATE_NOTIFICATION event is generated on the client.
Note: Before requesting a power profile schedule, the server application may send the schedule’s timing constraints to the client using the function eCLD_PPPowerProfileScheduleConstraintsNotificationSend(). The client application can alternatively request these schedule constraints from the server by calling eCLD_PPPowerProfileScheduleConstraintsReqSend().
Parent topic:Communicating schedule information