TwinCAT project setup

  1. Import the EtherCAT Subdevice Information (ESI) file of the FoE example.

  2. Copy the ESI filename ECAT-FOE.xml, generated by the SSC tool, from the SSC project folder to the <TwinCAT_installation_folder>/<Version>/Config/io/EtherCAT/ folder.

  3. Create a new project.

    1. Select File > New > Project.

      The New Project dialog box appears.

    2. Select TwinCAT Projects.

    3. Click OK.

  4. Scan for the subdevices.

    1. In the Solution Explorer view, expand I/O.

    2. Right-click on Device and select Scan.

      The scanned devices appear in theI/O devices found dialog box.

    3. Select the network interface connected with the FRDM-IMXRT1186 board.

    4. Click OK.

  5. Update the ESI file to E2PROM (You can skip this step if you ran EEPROM Update chapter).

    Note: The E2PROM must be updated if the FoE example is set up first time on the FRDM-IMXRT1186.

    1. Under Device, double-click Box1. The TwinCAT Project dialog box appears.

    2. Click the EtherCAT tab.

    3. Click the Advanced Settings button.

      The Advanced Settings dialog box appears.

    4. From the left pane of the Advanced Settings dialog box, select ESC Access > Smart View.

    5. Click the Write E2PROM button.

    6. From the available EEPROM list, select NXP > ECAT > foe.

    7. Click OK.

    8. Remove the device and rescan the device.

  6. Configure the subdevice.

    1. Click the DC tab.

    2. From the Operation Mode field, select the SM-Synchron or DC-Synchron option.

  7. Program the PLC code.

    1. In the Solution Explorer view, right-click on PLC.

    2. Select Add New Item.

      The Add New Item dialog box appears.

    3. From the Installed list in the left pane, select PLC Templates.

    4. Select Standard PLC Project.

    5. Click OK.

  8. To open the PLC edit page, select MAIN (PRG) under PLC.

  9. Copy the code below and paste it in the MAIN view.

    PROGRAM MAIN
    VAR 
    Delay : TON;
    LedIn AT %I* : BOOL; 
    LedOut AT %Q* : BOOL;
    END_VAR
    
    Delay(IN := TRUE, PT := T#1S);
    IF Delay.Q THEN
    LedOut := NOT LedIn;
    Delay(IN := FALSE);
    END_IF;
    

  10. To build the PLC code, right-click on the PLC project and select Build.

  11. Map the PLC variables to the subdevice IO channel.

    1. Right-click on MAIN.LedIn, select Change Link.

      The Attach Variable MAIN.LedIn (Input) dialog box appears.

    2. Select LED.

    3. Click OK.

    4. In the Solution Explorer, under PlcTask Outputs, right-click on MAIN.LedOut and select Change Link.

      The Attach Variable MAIN.LedOut (Output) dialog box appears.

    5. Select LED.

    6. Click OK.

  12. Activate Configuration

    1. To activate the configuration, select TwinCAT > Restart TwinCAT (Config Mode).

  13. FoE image upgrade.

    1. Click Device > Box1 > Online > Bootstrap.

    2. Click Download > ecat_foe_2-4-0_SIGNED.bin > Password’ > OK to upgrade the image.

      Note: FoE download Password: ‘12369874’.

      The serial terminal prints the following output.

      storage addr: 0x28240000
      FoE_StoreImage: processed 256 bytes
      FoE_StoreImage: processed 512 bytes
      ...
      FoE_StoreImage: upload complete (42028 bytes)
      write magic number offset = 0x43ff00
      Update image success
      
    3. After download, click ‘Init’ to restart the board.

      The serial terminal prints the following output.

      System reset...
      hello sbl.
      Bootloader Version 1.9.0
      Primary image: magic=good, swap_type=0x1, copy_done=0x3, image_ok=0x1
      Secondary image: magic=good, swap_type=0x1, copy_done=0x3, image_ok=0x3
      Boot source: none
      Swap type: test
      Starting swap using move algorithm.
      Bootloader chainload address offset: 0x40000
      Reset_Handler address offset: 0x40400
      Jumping to the image
      
      Start the SSC FoE example...
      Image version: 2.4.0
      Image state: testing
      Set image as confirmed: success
      
  14. FoE image download.

    1. Click Upload to choose the file to download.

  15. To download the upgraded image, click OK.

    Note: The download image name must be the same as the upgraded image name.