Changelog
All notable changes to NXP Bluetooth LE Host will be documented in this file.
NXP Bluetooth LE Host Stack is certified Bluetooth 6.0
[1.10.13] - mcux v2025-12-00-pvw2
Added
Threshold for the invalid number of Anchor Monitor events received by the target anchor
Experimental Monitoring Advertisers feature in Bluetooth LE Host
Experimental Randomized RPA feature in Bluetooth LE Host
Application defines for default connection and default advertising tx power
Improved
Miscellaneous applications updates
Central applications now wait for status of Encrypt procedure in case of bonded device
Logging data on localization applications
NBU Low Power Mode enabled by default for Localization Applications
PCT rotation calibration added to localization apps
Configured CS Reflector to start the CS procedure with the tdm command and updated the documentation
Populated the optionalSubfeaturesSupported field correctly
Prevented CORE 0 from entering deep sleep while LCE is computing by setting the low power mode constraint to PWR_WFI during LCE computation and releasing it afterwards
Implemented in CCC_CS, Channel Sounding data transfer from the anchor to the device
Documentation miscellaneous updates
Updated all kw47 and kw45 armgcc ld linker files to take gUseInternalStorageLink_d flag value into consideration
Fixed
Memory issue when setting scan response data would return an error status from the LL
Set advertises with the public address, overwritten by a previously used random address on receiving the Advertising Set Terminated event
Changed
Updated memory configuration: replaced the extended heap area in the available SMU2 memory with a 24KB array in the data1
Removed redundant cached remote capabilities write on reflectors, as the initiator will always trigger a capabilities exchange and trying to write cached capabilities afterwards results in an HCI error
Supported Platforms
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.12] - mcux v2025-12-00-pvw1
Added
Gap_LoadCustomBondedDeviceInformation API to retrieve custom peer information using NVM index
Improved
Miscellaneous application updates
Fixed
Updated privacy timeout mechanism affected by LE Set Extended Advertising Enable Command
Changed
Merged Gap_SetPeriodicAdvParameters and Gap_SetPeriodicAdvParametersV2 into Gap_SetPeriodicAdvParameters
Supported Platforms
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.11] - mcux v2025-09-00
Added
CCC sample applications updated to CCC Digital Key v4.0.0 Specification
RAS/RAP PTS 8.7.4 test support added in Localization Sample applications
Support for CS start procedure while the previous procedure is not completed; old procedure replaced with the new one
Support for arm gcc for ncp_loc_reader__cm33_core1
Improved
Localization Sample Applications Ram partition
RAS/RAP profile and service
Various sample applications have been updated
Fixed
Privacy setting issue on ncp_loc_reader
Extended NBU FSCI message handling issue
Ble_shell updated to set the Random Static Address properly
Always set the Advertising Legacy Set handle if the legacy API was used
fsci_bridge and w_uart_host memory leak
PAWR parameters in PeriodicSyncTransferReceived are now parsed correctly
Ensure an RPA/NRPA is properly set from the application to enable a central using Controller Privacy to connect to unbonded peripherals
CS algorithm buffer overwrite issue during Connection Handover application
Various sample applications bug fixes applied
Pass correct Codded PHY (S2) to Channel Sounding Set Procedure Parameters
Changed
Merged Gap_SetExtAdvertisingParameters and Gap_SetExtAdvertisingParametersV2 into Gap_SetExtAdvertisingParameters
ce_status_buffer type changed to int32_t
BLE_Shell prints Random Static address as identity address instead of the Public Device Address
Supported Platforms
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.10] - mcux v2025-09-00-pvw2
Improved
CS Event Handling: CS (Channel Sounding) events are now sent to the application task for processing, rather than being handled directly in the Host task
Various sample applications have been updated
Fixed
Bluetooth Advertising Sets: Now supports 4 advertising sets in the Bluetooth host libraries
Various sample applications bug fixes applied
Changed
Bluetooth Address Type: The default address type has been changed from Public to Random Static
Supported Platforms
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.9] - mcux v2025-09-00-pvw1
Added
IDS event trigger when incoming ATT packets exceed agreed MTU
IDS event trigger when Unexpected SMP Messages received in idle states (before pairing starts)
Average RSSI reporting in Anchor Monitor event
Support for gAppDeferAlgoRun_d in btcs_client.c
Multi-connection monitoring in Handover/Monitor Mode
Improved
Updated NBU channel sounding applications to support 64MHz clock speed
Cleanup of commComplete structures that only contain status from hci_interface.h
Fixed
CCC Application handover monitoring RSSI issue
Intrusion Detection System not reporting event type
Extended NBU armgcc projects stability
Advertising Extended Applications when Gap_PeriodicAdvCreateSync fails
Changed
Updated digital_key_car_anchor applications to configure coding scheme via Host API
Enhanced RAS handling of ACK Ranging Data in invalid conditions
Supported Platforms
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.8] - mcux v2025-06-00
Added
Gap_SetBondedDeviceName() to set device name using NVM index
RAS queue for GATT indications sent
gHciStatusBase_c to csError status
Option to use statically allocated memory for dynamic GATT database (prevents heap fragmentation)
Checks for controller supported features and setting PAST bits accordingly
Anchor support to export device data via RAS using gAppHciDataLogExport_d = 2
Anchor support to export device local HCI data using gAppHciDataLogExport_d = 1
Shell commands to list peer devices and trigger connection handover
Define for enabling optional CCC LE Coded PHY advertising
cs_sync_phy parameter to mDefaultRangeSettings (renamed from outdated RTTPhy)
Improved
Stack Host now saves the most recently set random address after successful controller response
Miscellaneous minor application updates
Fixed
Compilation issue in loc_reader app with real-time RAS transfer
CCC application handover state machine race condition
CCC resets gCurrentAdvHandle upon connection
RAS uses correct bit for data overwrite preference
Changed
Updated Bluetooth LE Host Documentation.
BLE_Shell Tx timer interval adjusted for max throughput on 1M PHY
CS_ConfigVendorCommand updated with Inline Phase Return field
Renamed tx_pwr_phy to phy and removed obsolete rtt_phy field
Updated documentation to clarify Controller Privacy restrictions
Supported Platforms
KW45, KW47, MCXW71, MCXW72, MCXW23
[1.10.7] - mcux v2025-06-00-pvw2
Added
Support for Bluetooth LE Debug Keys
Support for pairing failure reason 0x10 (Busy)
Extended NBU Wireless_uart_host battery service
Channel Sounding RSSI Information at application level
Application support for 4-antenna configuration
Improved
Clean include directives
Allow central-only devices to use Gap_EncryptAdvertisingData
CSTACK size optimization for RADE using baremetal apps
Fixed
Extended NBU memory leak issues
Issues when gAppOtaASyncFlashTransactions_c is set to 0
Issue with CS procedure affected by the CS data export
Extended NBU Wireless_uart_host privacy
Changed
Updated Bluetooth LE Host Documentation.
Supported Platforms
KW45, KW47, MCXW71, MCXW72, K32W1
[1.10.6] - mcux v2025-06-00-pvw1
Added
Encypted Advertising Data support in Extendded Advertising Applications.
Support for disable UART for CS applications for low power measurements.
Support for LCE (DSPV) non-blocking API integration to RADE.
Intrusion Detection System as Experimental.
Improved
L2CAP command length validation to cover all signaling commands.
Extended NBU Wireless_uart_host multiple connections support.
Supported Platforms
KW45, KW47, MCXW71, MCXW72, K32W1
[1.10.5] - mcux v2025-03-00
Added
MCXW72 Extended NBU support and w_uart_host, fsci_bridge and ncp_fscibb sample applications.
L2CAP support for Channel Sounding IQ Sample Transfer in CCC CS sample applications.
Bluetooth LE Sample applications for MCX-W71-EVK board.
Changed
Updated FSCI XML file.
Updated Bluetooth LE Host Documentation.
Fixed
Cleared the mpRemoteCachedCaps entry when the peer disconnects (CS sample applications).
Transfer RAS subscription data during connection handover (CCC CS sample applications).
EAD - Updated advertising data length check to ensure encrypted data fits inside one AD.
Updated digital_key_car_anchor and digital_key_car_anchor_cs applications to manage Random Static address from the application layer.
Supported Platforms
KW45, KW47, MCXW71, MCXW72, K32W1
[1.10.4] - mcux v2025-03-00-pvw2
Added
PAWR support in BLE Shell sample application.
PAWR support in adv_ext_peripheral and adv_ext_central sample applications.
New sample applications for FRDM-MCXW72.
Gap_SetScanningCallback API.
Support for handover connection interval update command.
Changed
Updated HID Device for Windows 11 compatibility.
Updated CCC demos to Digital Key R4 spec version 1.0.0.
Improved RPA resolution at the Host level, now performed synchronously.
Enhanced parsing of the CS procedure in Ranging Service.
Fixed
Corrected parsing of the PAST command in FSCI GAP.
Fixed scan event reporting in PAST scenario.
Added an error case for
Gap_SetChannelMapin the generic event handler.
Supported Platforms
KW45, KW47, MCXW71, MCXW72, K32W1