Hardware requirements#
Mini/micro USB cable
MIMXRT1060-EVKC board
Personal Computer
Headphone(OMTP standard)
CS42448 Audio board
Board settings#
Make sure R113 is welded on MIMXRT1060-EVKC board. Insert AUDIO board into J23.
Prepare the Demo#
Note: The demo support CS42448 codec only.
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Insert the headphones into the headphone jack J6 or J7 on the audio board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
Note: This demo outputs 1KHZ sine wave audio signal. When the demo runs successfully, you can hear the tone playback from J6/J7 and the log would be seen on the OpenSDA terminal like:
SAI EDMA multi channel transfer example started!
SAI EDMA multi channel transfer example finished!