MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MIMX8MQ6-EVK board

  • J-Link Debug Probe

  • 12V power supply

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect 12V power supply and J-Link Debug Probe to the board, switch SW701 to power on the board

  2. Connect a USB cable between the host PC and the J1701 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the demo.

Running the demo#

The log below shows the output of the hello world demo in the terminal window:

TMU monitor report example.
site 1 immediate temperature is too high. 41°C
site 1 immediate temperature is too high. 41°C
site 0 immediate temperature is too high. 41°C
site 1 immediate temperature is too high. 42°C
site 0 immediate temperature is too high. 41°C
site 1 immediate temperature is too high. 42°C
...