Hardware requirements#
Micro USB cable
MIMX8ULP-EVK/EVK9 board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the example with with imx-mkimage.(Not running it with your IDE, unless it will be failed to running). Note: After a successful execution, if you need to execute again, you need to completely power down the board and restart it again.
Running the demo#
The log below shows the output of the powerquad_fir_fast example in the terminal window:
BOARD_ReleaseTRDC: 75 start release trdc
BOARD_ReleaseTRDC: 78 finished release trdc, status = 0xd6
BOARD_SetTrdcGlobalConfig: 93 start setup trdc
BOARD_SetTrdcGlobalConfig: 402 finished setup trdc
POWERQUAD FIR fast example started
PQ fir fixed 16-bit normal method: xxx
PQ fir fixed 16-bit fast method: xxx
PQ fir fixed 32-bit normal method: xxx
PQ fir fixed 32-bit fast method: xxx
PQ fir float normal method: xxx
PQ fir float fast method: xxx
PQ conv fixed 16-bit normal method: xxx
PQ conv fixed 16-bit fast method: xxx
PQ conv fixed 32-bit normal method: xxx
PQ conv fixed 32-bit fast method: xxx
PQ conv float normal method: xxx
PQ conv float fast method: xxx
PQ corr fixed 16-bit normal method: xxx
PQ corr fixed 16-bit fast method: xxx
PQ corr fixed 32-bit normal method: xxx
PQ corr fixed 32-bit fast method: xxx
PQ corr float normal method: xxx
PQ corr float fast method: xxx
POWERQUAD FIR fast example successed