Hardware requirements#
Mini/micro USB cable
MIMXRT1160-EVK board
Personal Computer
RK055AHD091 panel or RK055MHD091 panel
OV5640 camera
Board settings#
Connect the panel to J48 Connect camera to J2 Connect 5V power to J43, set J38 to 1-2
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Build the project, this project uses RK055MHD091 panel by default, to use the RK055AHD091 panel, change #define DEMO_PANEL 2 to #define DEMO_PANEL 0 in mcux_config.h.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs, the screen shows the camera input frame.