MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • EVK-MIMXRT595 board

  • Personal Computer

Board settings#

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

When the example runs successfully, you can see the similar information from the terminal as below.

I2C example -- Read Accelerometer Value
Found an FXOS8700 on board , the device address is 0x1e .
The accel values:
status_reg = 0xff , x =    20 , y =  -102 , z =  2102
status_reg = 0xff , x =    83 , y =   -51 , z =  2089
status_reg = 0xff , x =    66 , y =   -53 , z =  2101
status_reg = 0xff , x =    51 , y =   -80 , z =  2098
status_reg = 0xff , x =    15 , y =   -99 , z =  2105
status_reg = 0xff , x =    44 , y =   -89 , z =  2097
status_reg = 0xff , x =    53 , y =   -56 , z =  2099
status_reg = 0xff , x =    54 , y =   -78 , z =  2103
status_reg = 0xff , x =    25 , y =   -98 , z =  2098
status_reg = 0xff , x =    17 , y =  -118 , z =  2107

End of I2C example .