Hardware requirements#
Micro USB cable
EVK-MIMXRT685 board
Personal Computer
headphones with 3.5 mm stereo jack
source of sound (line output to 3.5 mm stereo jack)
Board settings#
To make example work, connections needed to be as follows: JP7-1 <–> JP7-2 JP8-1 <–> JP8-2
Prepare the Demo#
Connect headphones to Audio HP / Line-Out connector (J4).
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
Headphones will play a sine wave sound. This demo outputs 450HZ sine wave audio signal. The log below shows example output of the I2S driver demo in the terminal window:
Configure codec
Configure I2S
Setup looping playback of sine wave