MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-MCXL255 board

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a Type-C USB cable between the host PC and the MCU-Link port (J16) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

The following lines are printed to the serial terminal when the demo program is executed.

USART CMSIS interrupt example
Board receives 8 characters then sends them out
Now please input: