Hardware requirements#
Mini/micro USB cable
KW45B41Z-EVK Board
Personal Computer
Board settings#
No special is needed.
Prepare the Demo#
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the OpenSDA terminal like::
Lpuart interrupt example with seven data bits
Board receives 8 characters then sends them out
Now please input: