Hardware requirements#
Micro USB cable
LPCXpresso54S018M board
Personal Computer
Board settings#
To make i2c example work, connections needed to be as follows: I2C8 connected to I2C9 SCL P1_18(J9 pin2) –> P3_22(J9 pin11) SDA P1_17(J9 pin4) –> P3_21(J9 pin13)
Prepare the Demo#
Connect a micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.
Open a serial terminal on PC for JLink serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.