Hardware requirements#
Mini/micro USB cable
LPCXpresso55S16 board
Personal Computer
headphones with 3.5 mm stereo jack
source of sound (line output to 3.5 mm stereo jack)
Board settings#
The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)
Prepare the Demo#
Connect headphones to Audio HP / Line-Out connector.
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board
Open a serial terminal with the following settings :
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
Headphones will play a sine wave sound. This demo outputs 450HZ sine wave audio signal. The log below shows example output of the I2S driver demo in the terminal window:
Configure I2C
Configure codec
Configure I2S
Setup looping playback of sine wave
Modify i2s_interrupt_transfer.c to change condition to call StartDigitalLoopback() instead of StartSoundPlayback() function. Headphones will play what is input into Audio Line-In connector. Terminal window will show:
Configure codec
Configure I2S
Setup digital loopback