Hardware requirements#
USB Type-C cable
Network cable RJ45 standard
MCIMX93AUTO-EVK board
Personal Computer
Board settings#
This example uses 1G port(J601) as default.
Note#
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.