MCUXpresso SDK Documentation

Hardware requirements#

  • USB Type-C cable

  • MCIMX93-QSB board

  • Personal Computer

Board settings#

Populate R1010 with 10KΩ

Note#

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

Prepare the Demo#

  1. Connect 12V~20V power supply and JLink Plus to the board, switch SW301 to power on the board

  2. Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

The following message shows in the terminal if the example runs successfully.

I3C master read sensor data example.

Start to do I3C master transfer in SDR mode.

Success to read WHO_AM_I register value from LSDM6DSO on board in I3C SDR mode, the value is 0x6C.
~~~~~~~~~~~~~~~~~~~~~~~~~~~