Hardware requirements#
Mini/micro USB cable
MIMXRT700-EVK board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect the PC host and the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the hello world multicore demo in the terminal window:
Starting Secondary core.
Hello World from the Primary Core!