MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MIMXRT685-AUD-EVK board

  • Personal Computer

Board settings#

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

The log below shows the output of the pca9420 example in the terminal window, and user can interact with the application in terminal:

-------------- PCA9420 on board PMIC driver example --------------

Please select the PMIC example you want to run:
[1]. Dumping Mode Settings
[2]. Switch Mode
[3]. Dumping Selected Register Content
[4]. Feed watch dog

Note: Example enable watchdog power in mode 3, so it will timerout after 16 seconds unless keep call Feed watch dog example.