MCUXpresso SDK Documentation

MCUXpresso SDK Release Notes#

Overview#

The MCUXpresso SDK is a comprehensive software enablement package designed to simplify and accelerate application development with Arm Cortex-M-based devices from NXP, including its general purpose, crossover and Bluetooth-enabled MCUs. MCUXpresso SW and Tools for DSC further extends the SDK support to current 32-bit Digital Signal Controllers. The MCUXpresso SDK includes production-grade software with integrated RTOS (optional), integrated enabling software technologies (stacks and middleware), reference software, and more.

In addition to working seamlessly with the MCUXpresso IDE, the MCUXpresso SDK also supports and provides example projects for various toolchains. The Development tools chapter in the associated Release Notes provides details about toolchain support for your board. Support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.

Underscoring our commitment to high quality, the MCUXpresso SDK is MISRA compliant and checked with Coverity static analysis tools. For details on MCUXpresso SDK, see MCUXpresso-SDK: Software Development Kit for MCUXpresso.

MCUXpresso SDK#

As part of the MCUXpresso software and tools, MCUXpresso SDK is the evolution of Kinetis SDK, includes support for LPC, DSC,PN76, and i.MX System-on-Chip (SoC). The same drivers, APIs, and middleware are still available with support for Kinetis, LPC, DSC, and i.MX silicon. The MCUXpresso SDK adds support for the MCUXpresso IDE, an Eclipse-based toolchain that works with all MCUXpresso SDKs. Easily import your SDK into the new toolchain to access to all of the available components, examples, and demos for your target silicon. In addition to the MCUXpresso IDE, support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.

In order to maintain compatibility with legacy Freescale code, the filenames and source code in MCUXpresso SDK containing the legacy Freescale prefix FSL has been left as is. The FSL prefix has been redefined as the NXP Foundation Software Library.

Development tools#

The MCUXpresso SDK was tested with following development tools. Same versions or above are recommended.

  • MCUXpresso IDE, Rev. 25.06.xx

  • IAR Embedded Workbench for Arm, version is 9.70.2

  • Keil MDK, version is 5.42a

  • MCUXpresso for VS Code v26.03

  • GCC Arm Embedded Toolchain 14.2.x

Supported development systems#

This release supports board and devices listed in following table. The board and devices in bold were tested in this release.

Development boards

MCU devices

LPCXpresso51U68

LPC51U68JBD48, LPC51U68JBD64

MCUXpresso SDK release package#

The MCUXpresso SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, CMSIS, devices, middleware, and RTOS support.

Device support#

The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.

Board support#

The boards folder provides the board-specific demo applications, driver examples, and middleware examples.

Demo application and other examples#

The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.

RTOS#

FreeRTOS#

Real-time operating system for microcontrollers from Amazon

Middleware#

CMSIS DSP Library#

The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.

coreHTTP#

coreHTTP

USB Type-C PD Stack#

See the MCUXpresso SDK USB Type-C PD Stack User’s Guide (document MCUXSDKUSBPDUG) for more information

USB Host, Device, OTG Stack#

See the MCUXpresso SDK USB Stack User’s Guide (document MCUXSDKUSBSUG) for more information.

TinyCBOR#

Concise Binary Object Representation (CBOR) Library

PKCS#11#

The PKCS#11 standard specifies an application programming interface (API), called “Cryptoki,” for devices that hold cryptographic information and perform cryptographic functions. Cryptoki follows a simple object based approach, addressing the goals of technology independence (any kind of device) and resource sharing (multiple applications accessing multiple devices), presenting to applications a common, logical view of the device called a “cryptographic token”.

LVGL#

LVGL Open Source Graphics Library

llhttp#

HTTP parser llhttp

FreeMASTER#

FreeMASTER communication driver for 32-bit platforms.

emWin#

The MCUXpresso SDK is pre-integrated with the SEGGER emWin GUI middleware. The AppWizard provides developers and designers with a flexible tool to create stunning user interface applications, without writing any code.

Release contents#

Provides an overview of the MCUXpresso SDK release package contents and locations.

Deliverable

Location

Boards

INSTALL_DIR/boards

Demo Applications

INSTALL_DIR/boards/<board_name>/demo_apps

Driver Examples

INSTALL_DIR/boards/<board_name>/driver_examples

eIQ examples

INSTALL_DIR/boards/<board_name>/eiq_examples

Board Project Template for MCUXpresso IDE NPW

INSTALL_DIR/boards/<board_name>/project_template

Driver, SoC header files, extension header files and feature header files, utilities

INSTALL_DIR/devices/<device_name>

CMSIS drivers

INSTALL_DIR/devices/<device_name>/cmsis_drivers

Peripheral drivers

INSTALL_DIR/devices/<device_name>/drivers

Toolchain linker files and startup code

INSTALL_DIR/devices/<device_name>/<toolchain_name>

Utilities such as debug console

INSTALL_DIR/devices/<device_name>/utilities

Device Project Template for MCUXpresso IDE NPW

INSTALL_DIR/devices/<device_name>/project_template

CMSIS Arm Cortex-M header files, DSP library source

INSTALL_DIR/CMSIS

Components and board device drivers

INSTALL_DIR/components

RTOS

INSTALL_DIR/rtos

Release Notes, Getting Started Document and other documents

INSTALL_DIR/docs

Tools such as shared cmake files

INSTALL_DIR/tools

Middleware

INSTALL_DIR/middleware

Known issues#

This section lists the known issues, limitations, and/or workarounds.

Cannot add SDK components into FreeRTOS projects#

It is not possible to add any SDK components into FreeRTOS project using the MCUXpresso IDE New Project wizard.