MCUXpresso SDK Documentation

Hardware requirements#

  • Mini/micro USB cable

  • MIMXRT1170-EVKB board

  • Personal Computer

  • Headphone(OMTP standard)

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Insert the headphones into the headphone jack on MIMXRT1170-EVKB board (J101).

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

When the demo runs successfully, you can hear the tone and the log would be seen on the OpenSDA terminal like:

ASRC m2m polling example

Playback raw audio data

    sample rate : xxxx

    channel number: xxxx

    frequency: xxxx.


Playback converted audio data

    sample rate : xxxx

    channel number: xxxx

    frequency: xxxx.

ASRC m2m polling example finished