Hardware requirements#
Mini/micro USB cable
MIMXRT1160-EVK board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the PC host and the OpenSDA USB on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
When the example runs successfully, following information can be seen on the OpenSDA terminal:
==FlexCAN loopback example -- Start.==
Send message from MB8 to MB9
tx word0 = 0x11223344
tx word1 = 0x55667788
Received message from MB9
rx word0 = 0x11223344
rx word1 = 0x55667788
==FlexCAN loopback example -- Finish.==