MCUXpresso SDK Documentation

Hardware requirements

Hardware requirements#

  • Micro USB cable

  • EVK-MIMXRT595 board

  • Personal Computer

Board settings#

No special settings are required.

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

The log below shows example output of the SCTimer driver simple PWM demo in the terminal window:

SCTimer example to output edge-aligned PWM signal

When user presses a switch the PWM signal will be seen from Out 3
When user presses the switch again PWM signal on Out 3 will turn off
The PWM signal from Out 0 will remain active all the time

Use Oscilloscope to measure and observe the J30-1(out 0) and J30-2(out 1) output signal, use SW2 as switch.