MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-KW43 Board

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the FRDM board J28.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

When the example runs successfully, following information can be seen on the terminal:


==FlexCAN loopback example -- Start.==

Send message from MB1 to MB0
tx word0 = 0x11223344
tx word1 = 0x55667788

Received message from MB0
rx word0 = 0x11223344
rx word1 = 0x55667788

==FlexCAN loopback example -- Finish.==