MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-MCXA577 board

  • Personal Computer

  • Loopback network cable RJ45 standard

Board settings#

Short position 2-3 on J29.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Insert loopback network cable to Ethernet RJ45 port.

  4. Download the program to the target board.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

The example uses external PHY over RMII by default. If you want to use the internal 10BASE-T1S digital PHY, redefine BOARD_NETWORK_USE_TENBASET_PHY from board.h to 1 and rebuild. Loopback cable is not needed in that case.

Make loopback network cable:

Pin

568B standard

Unknown standard

J1

orange+white

green+white

J2

orange

green

J3

green+white

orange+white

J4

blue

brown+white

J5

blue+white

brown

J6

green

orange

J7

brown+white

blue

J8

brown

blue+white

Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not shown in the list, please connect J1~J8 based on your situation.

Running the demo#

The log below shows example output of the example in the terminal window:


ENET example start.
Wait for PHY init...
Wait for PHY link up...

Transmission start now!
The 1-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 2-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 3-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 4-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 5-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 6-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 7-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 8-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 9-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 10-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 11-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 12-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 13-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 14-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 15-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 16-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 17-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 18-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 19-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff
The 20-th frame transmitted success!
 One frame received. the length 1018
 Dest Address ff:ff:ff:ff:ff:ff Src Address 54:27:8d:ff:ff:ff