Hardware requirements#
Type-C USB cable
FRDM-MCXA577 Board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect the type-C USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, following information can be seen on the terminal:
==FlexCAN loopback example -- Start.==
Send message from MB0 to MB1
tx word0 = 0x11223344
tx word1 = 0x55667788
Received message from MB1
rx word0 = 0x11223344
rx word1 = 0x55667788
==FlexCAN loopback example -- Finish.==