MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-MCXW71 Board

  • Personal Computer

Board settings#

The example requires 2 sets of boards, each of them is mounted with the base board. To make example work, connections needed to be as follows on each base board:

Board to board connections needed to be as follows:

        Node A           connect to      Node B
Pin Name   Board Location         Pin Name    Board Location
CANH       J21-1                  CANH        J21-1
CANL       J21-2                  CANL        J21-2
GND        J21-4                  GND         J21-4

Prepare the Demo#

  1. Connect the micro and mini USB cable between the PC host and the USB ports on the board.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

After connecting the two boards, these instructions display on each terminal window. One board must be chosen as node A and the other board as node B. (Note: Node B should start first) Data is sent continuously between the node A and the node B.

This message displays on the node A terminal:

FlexCAN pretended networking wake up example.
Please select local node as A or B:
Note: Node B should start first.
Node:a
Press any key to trigger one-shot transmission
Send message ID: 0x123, payload: 0x0055000000000000

Press any key to trigger the next transmission!
Send message ID: 0x123, payload: 0x0155000000000000

Press any key to trigger the next transmission!
Send message ID: 0x125, payload: 0x0255000000000000

Press any key to trigger the next transmission!
Send message ID: 0x125, payload: 0x0355000000000000

Press any key to trigger the next transmission!
Send message ID: 0x123, payload: 0x0455000000000000

Press any key to trigger the next transmission!
Send message ID: 0x123, payload: 0x0056000000000000

...

This message displays on the node B terminal:

FlexCAN pretended networking wake up example. Please select local node as A or B: Note: Node B should start first. Node:b Note B will enter lower power mode and wake up until received 4 specific messages. Wake up message format: Standard (11 bit id) Wake up message ID range: 0x123 to 0x124 Wake up payload range : 0x0055000000000000 to 0x0056000000000000 Waken up! Match message 0 ID: 0x123, payload: 0x0055000000000000 Match message 1 ID: 0x123, payload: 0x0155000000000000 Match message 2 ID: 0x123, payload: 0x0455000000000000 Match message 3 ID: 0x123, payload: 0x0056000000000000 Enter lower power mode again!