Hardware requirements#
Mini/micro USB cable
IMX943-EVK board
Personal Computer
Oscilloscope
Board settings#
Probe the pwm signal using an oscilloscope
At J49-15 (PWM Submodule0)
At J49-11 (PWM Submodule1)
At J49-7 (PWM Submodule2)
J45-12 (GND)
Prepare the Demo#
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
IPSYNC trigger signal connected!
FlexPWM driver example
~~~~~~~~~~~~~~~~~~~~~~~
You can capture the PWM on OSC with trigger signal. If disable trigger signal from XBAR, the PWM will not be get on OSC.