Hardware requirements#
Micro USB cable
LPCXpresso51U68 board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo#
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The following lines are printed to the serial terminal when the demo program is executed.
IAP Flash example
Writing flash sector 1
Erasing flash sector 1
Erasing page 1 in flash sector 1
Entire flash signature
XXXXXXXX
End of IAP Flash Example