Hardware requirements#
Micro USB cable
LPCXpresso51U68 board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo#
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The following lines are printed to the serial terminal when the demo program is executed.
PINT Pattern Match example
PINT Pattern match events are configured
Press corresponding switches to generate events
This example configures “Pin Interrupt 0” to be invoked when SW1 switch is pressed by the user. Bit slice 0 is configured as an endpoint in sticky falling edge mode. The interrupt callback prints “PINT Pin Interrupt 0 event detected. PatternMatch status = 1”.
“Pin Interrupt 2” is configured to be invoked when rising edge on SW1, SW2 is detected. The interrupt callback prints “PINT Pin Interrupt 2 event detected. PatternMatch status = 100”. Bit slices 1 configured to detect sticky rising edge. Bit slice 2 is configured as an endpoint.