Hardware requirements#
Micro USB cable
LPCXpresso54S018 board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo#
This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:
Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”
This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):
a. Open SEGGER J-FLASH Lite, select device LPC54S018.
b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)
c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
Launch the debugger in your IDE to begin running the demo.
The following lines are printed to the serial terminal when the demo program is executed.
PINT Pin interrupt example
PINT Pin Interrupt events are configured
Press corresponding switches to generate events
This example configures “Pin Interrupt 0” to be invoked when SW2 switch is pressed by the user. The interrupt callback prints “PINT Pin Interrupt 0 event detected”. “Pin Interrupt 1” is is configured to be invoked when SW3 is pressed. The interrupt callback prints “PINT Pin Interrupt 1 event detected”. “Pin Interrupt 2” is configured to be invoked when SW4 is pressed. The interrupt callback prints “PINT Pin Interrupt 2 event detected”.