Hardware requirements#
Mini/micro USB cable
LPCXpresso55S28 board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
DMA hardware trigger example begin.
Destination Buffer:
0 0 0 0
Press SW1 to trigger one shot DMA transfer.
SW1 is pressed.
DMA hardware trigger example finish.
Destination Buffer:
1 2 3 4