Hardware requirements#
Micro USB cable
LPCXpresso802 board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a micro USB cable between the host PC and the CMSIS DAP port(CN1 on the board).
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo#
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The following lines are printed to the serial terminal when the demo program is executed.
IAP Flash example
Writing flash sector 1
Erasing flash sector 1
Erasing page 1 in flash sector 1
Flash signature value of page 1
XXXXXXXXXXXXXXXXXXXXX
End of IAP Flash Example