Hardware requirements#
Mini/micro USB cable
LPCXpresso845MAX board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
DMA memory to memory polling example begin.
Destination Buffer:
0 0 0 0
DMA memory to memory polling example finish.
Destination Buffer:
1 2 3 4