MCUXpresso SDK Documentation

i.MX RT bootable image#

Bootable image layout in target flash device#

There are two types of supported boot image:

  • XIP (Execute-In-Place) boot image: This type of boot image is only applicable to Serial NOR devices connected to QuadSPI or FlexSPI interfaces and Parallel NOR devices connected to WEIM or SEMC interface. The boot device memory is identical to the destination memory. ROM can boot this boot image directly.

  • Non-XIP boot image: This type of boot image is usually for the NAND, SD, and eMMC devices. The boot device memory is different from the destination memory. ROM loads the boot image from the boot device memory to the destination memory and then boots from the destination memory.

Bootable image layout

Boot image format#

This section describes the boot image format and data structures. The elftosb utility helps the customers automatically generate the boot image format file. The elftosb utility usage is described later in this document.

The bootable image must have the following data structures:

  • Image Vector Table (IVT): a list of pointers located at a fixed address that ROM examines to determine the location of other components of the bootable image

  • Boot Data: a table that indicates the bootable image location, image size in bytes, and the plugin flag

  • Device configuration data (DCD) (optional): IC configuration data configures DDR/SDRAM memory

  • User application and data

  • CSF (optional): signature block for Secure Boot generated by CST

  • KeyBlob (optional): a data structure consists of wrapped DEK for encrypt boot

Each bootable image starts with appropriate IVT. In general, for the external memory devices that support XIP feature, the IVT offset is 0x1000 else it is 0x400.

IVT and boot data#

The IVT is the data structure that the BootROM reads from the boot devices. This data structure supplies the bootable image containing the required data components to perform a successful boot.

See the Program image section in the System Boot chapter of the device reference manual for more details.

IVT data structure

Offset

Field

Description

0x00 - 0x03

header

•   Byte 0 tag, fixed to 0xD1

•   Byte 1,2 length, bit endian format containing the overall length of the IVT in bytes, fixed to 0x00, 0x20

•   Byte 3: version, valid values: 0x40, 0x41, 0x42, 0x43

0x04 - 0x07

entry

Absolute address of the first instruction to execute from the image, or the vector address of the image

0x08 - 0x0b

reserved1

Reserved for future use, set to 0

0x0c - 0x0f

dcd

Absolute address of the image DCD. It is optional, so this field can be set to NULL if no DCD is required

0x10 - 0x13

boot_data

Absolute address of the boot data

0x14 - 0x17

self

Absolute address of the IVT

0x18 - 0x1b

csf

Absolute address of the Command Sequence File (CSF) used by the HAB library

0x1c - 0x1f

reserved2

Reserved, set to 0

Boot data structure#

Boot data structure

Offset

Field

Description

0x00-0x03

start

Absolute address of the bootable image

0x04-0x07

length

Size of the bootable image

0x08-0x0b

plugin

Plugin flag, set to 0 because plugin boot is not supported on the this device

Signed image#

The bootable image can be signed by CST tool. The tool generates the CSF data in the binary file format that consists of command sequences and signatures based on given input command sequence file (csf file). Refer to the documentation in the CST release package for further details.

In this document, a simple method is introduced to generate signed images using the elftosb utility.

Encrypted image#

There are two types of encrypted image formats:

Encrypted XIP image format

The Flashloader generates the encrypted XIP image using the AES CTR algorithm when programming the image on the device. On execution, the hardware engine does on-the-fly decryption.

Encrypted image generated by CST

To increase the security level, the bootable image can be signed and further encrypted by the CST. The KeyBlob must be generated on the device. The hardware deletes all sensitive keys if any security violation happens so that the sensitive keys cannot be cloned.

In this document, a simple method is introduced to generate signed images using the elftosb utility.