Hardware requirements
=====================
- Type-C USB cable
- FRDM-MCXW72 Board
- Personal Computer

Board settings
==============
No special settings are required.

Prepare the Demo
================
1. Connect a USB cable between the host PC and the FRDM board J10.
2. Open a serial terminal on PC for the serial device with these settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3. Download the program to the target board.
4. Either press the reset button on your board or launch the debugger in your IDE to begin running
   the demo.

Running the demo
================
When the example runs successfully, the following message is displayed in the terminal:
~~~~~~~~~~~~~~~~~~~~~
EDMA scatter_gather transfer example begin.

Destination Buffer:
0       0       0       0       0       0       0       0

EDMA scatter_gather transfer example finish.

Destination Buffer:
1       2       3       4       5       6       7       8
~~~~~~~~~~~~~~~~~~~~~