# cmsis_uart_edma_transfer

## Overview
CMSIS-Driver defines generic peripheral driver interfaces for middleware making it reusable across a wide
range of supported microcontroller devices. The API connects microcontroller peripherals with middleware
that implements for example communication stacks, file systems, or graphic user interfaces.
More information and usage method please refer to http://www.keil.com/pack/doc/cmsis/Driver/html/index.html.

The cmsis_uart_edma_transfer example shows how to use uart cmsis  driver with EDMA:

In this example, one uart instance connect to PC through uart, the board will
send back all characters that PC send to the board.

Note: The example echo every 8 characters, so input 8 characters every time.

## Supported Boards

````{container} board-selector

```{container} board-setup
:name: board-frdmk22f

##### FRDM-K22F

##### Hardware requirements
- Mini/Micro USB cable
- FRDM-K22F board
- Personal Computer

##### Board settings
No special is needed.

##### Prepare the Demo
1.  Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
2.  Open a serial terminal on PC for OpenSDA serial device with these settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Reset the SoC and run the project.

##### Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

~~~~~~~~~~~~~~~~~~~~~~~~~~~
USART EDMA example
Send back received data
Echo every 8 characters

~~~~~~~~~~~~~~~~~~~~~~~~~~~

```

```{container} board-setup
:name: board-frdmke17z512

##### FRDM-KE17Z512

##### Hardware requirements
- Micro USB cable
- FRDM-KE17Z512 board
- Personal Computer
- USB to Com converter

##### Board settings
J4-10 connect to TxD of the USB to Com converter.
J4-12 connect to RxD of the USB to Com converter.
J3-14 connect to GND of the USB to Com converter 

##### Prepare the Demo
1.  Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo
When the example runs successfully, the following message is displayed in the terminal:

~~~~~~~~~~~~~~~~~~~~~~~
UART EDMA example
Send back received data
Echo every 8 characters
~~~~~~~~~~~~~~~~~~~~~~~

When you input 8 characters, system will echo it by UART and them would be seen on the MCU-LINK terminal.

```

````