# led_blinky_1

## Overview
The LED Blinky demo application provides a sanity check for the new SDK build environments and board bring up. The LED Blinky demo 
uses the systick interrupt to realize the function of timing delay. The example takes turns to shine the LED. The purpose of this 
demo is to provide a simple project for debugging and further development.
The code of this demo has been prepared and updated for use with the MCUXpresso Configuration Tools (Pins/Clocks/Peripherals).

## Supported Boards

````{container} board-selector

```{container} board-setup
:name: board-frdmke02z40m

##### FRDM-KE02Z40M

##### Hardware requirements
- Mini USB cable
- FRDM-KE02z40m board
- Personal Computer

##### Board settings
This example project does not call for any special hardware configurations.
Although not required, the recommendation is to leave the development board's jumper settings
and configurations in default state when running this example.

##### Prepare the Demo
1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.
2. Download the program to the target board.
3. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo
When the demo runs successfully, you will find the LED is blinking.

```

````