# aoi_io_and

## Overview
The AOI IO_AND demo application demonstrates the use of IO and AOI peripherals.
The example Use the two IO as the input of the aoi function: AOI_OUT = (IO0 & IO1). 
When IO0 and IO1 are both high level, the AOI_OUT is high level.
When any of IO is low level, the AOI_OUT is low level.
The purpose of this demonstration is to show how to use the AOI driver in the SDK software.

## Run the demo

After the demonstration runs successfully, you can see the following information in the terminal window:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
aoi_io_and project.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

## Supported Boards

````{container} board-selector

```{container} board-setup
:name: board-frdmmcxa153

##### FRDM-MCXA153

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXA153 board
- Personal Computer

##### Board settings
AOI_OUT = EXT_TRIG_OUT0 P1_2 J6-5
IO0     = EXT_TRIG_IN0 P1_0 J6-6
IO1     = EXT_TRIG_IN1 P1_1 J6-4

AOI_OUT = IO0 & IO1

##### Prepare the Demo
1.  Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo

The log below shows the output of the aoi demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
AOI_io_and project.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

When IO0 and IO1 are both high level, the AOI_OUT is high level.
When any of IO is low level, the AOI_OUT is low level.

```

```{container} board-setup
:name: board-frdmmcxa156

##### FRDM-MCXA156

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXA156 board
- Personal Computer

##### Board settings
AOI_OUT = EXT_TRIG_OUT0 P1_2 J6-5
IO0     = EXT_TRIG_IN0 P1_0 J6-6
IO1     = EXT_TRIG_IN1 P1_1 J6-4

AOI_OUT = IO0 & IO1

##### Prepare the Demo
1.  Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo

The log below shows the output of the aoi demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
AOI_io_and project.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

When IO0 and IO1 are both high level, the AOI_OUT is high level.
When any of IO is low level, the AOI_OUT is low level.

```

```{container} board-setup
:name: board-frdmmcxa346

##### FRDM-MCXA346

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXA346 board
- Personal Computer

##### Board settings
AOI_OUT = EXT_TRIG_OUT0 P1_2 J6-5
IO0     = EXT_TRIG_IN0 P1_0 J6-6
IO1     = EXT_TRIG_IN1 P1_1 J6-4

AOI_OUT = IO0 & IO1

##### Prepare the Demo
1.  Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo

The log below shows the output of the aoi demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
AOI_io_and project.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

When IO0 and IO1 are both high level, the AOI_OUT is high level.
When any of IO is low level, the AOI_OUT is low level.

```

```{container} board-setup
:name: board-frdmmcxl255

##### FRDM-MCXL255

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXL255 board
- Personal Computer

##### Board settings
IO0     = EXT_TRIG_IN1 P1_18 J2
IO1     = EXT_TRIG_IN2 P1_19 J2
AOI_OUT = EXT_TRIG_OUT0 P3_8 J1

AOI_OUT = IO0 & IO1

##### Prepare the Demo
1.  Connect a USB Type-C cable between the host PC and the MCU-Link USB port (J16) on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo
When IO0 and IO1 are both high level, the AOI_OUT is high level.
When any of IO is low level, the AOI_OUT is low level.

The following lines are printed to the serial terminal when the demo program is executed.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
aoi_io_and project.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

```

```{container} board-setup
:name: board-frdmmcxa174

##### FRDM-MCXA174

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXA174 board
- Personal Computer

##### Board settings
AOI_OUT = EXT_TRIG_OUT0 P1_2 J6-5
IO0     = EXT_TRIG_IN0 P1_0 J6-6
IO1     = EXT_TRIG_IN1 P1_1 J6-4

AOI_OUT = IO0 & IO1

Short JP7

##### Prepare the Demo
1.  Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo

The log below shows the output of the aoi demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
AOI_io_and project.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

When IO0 and IO1 are both high level, the AOI_OUT is high level.
When any of IO is low level, the AOI_OUT is low level.

```

```{container} board-setup
:name: board-frdmmcxa344

##### FRDM-MCXA344

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXA344 board
- Personal Computer

##### Board settings
AOI_OUT = EXT_TRIG_OUT0 P1_2 J6-5
IO0     = EXT_TRIG_IN0 P1_0 J6-6
IO1     = EXT_TRIG_IN1 P1_1 J6-4

AOI_OUT = IO0 & IO1

Short JP7

##### Prepare the Demo
1.  Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo

The log below shows the output of the aoi demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
AOI_io_and project.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

When IO0 and IO1 are both high level, the AOI_OUT is high level.
When any of IO is low level, the AOI_OUT is low level.

```

```{container} board-setup
:name: board-frdmmcxa266

##### FRDM-MCXA266

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXA266 board
- Personal Computer

##### Board settings
AOI_OUT = EXT_TRIG_OUT0 P1_2 J6-5
IO0     = EXT_TRIG_IN0 P1_0 J6-6
IO1     = EXT_TRIG_IN1 P1_1 J6-4

AOI_OUT = IO0 & IO1

##### Prepare the Demo
1.  Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo

The log below shows the output of the aoi demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
AOI_io_and project.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

When IO0 and IO1 are both high level, the AOI_OUT is high level.
When any of IO is low level, the AOI_OUT is low level.

```

```{container} board-setup
:name: board-frdmmcxa366

##### FRDM-MCXA366

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXA366 board
- Personal Computer

##### Board settings
AOI_OUT = EXT_TRIG_OUT0 P1_2 J6-5
IO0     = EXT_TRIG_IN0 P1_0 J6-6
IO1     = EXT_TRIG_IN1 P1_1 J6-4

AOI_OUT = IO0 & IO1

##### Prepare the Demo
1.  Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo

The log below shows the output of the aoi demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
AOI_io_and project.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

When IO0 and IO1 are both high level, the AOI_OUT is high level.
When any of IO is low level, the AOI_OUT is low level.

```

```{container} board-setup
:name: board-frdmmcxa577

##### FRDM-MCXA577

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXA577 board
- Personal Computer

##### Board settings
AOI_OUT = EXT_TRIG_OUT3 P4_5 J6-5
IO0     = EXT_TRIG_IN10 P5_5 J2-15
IO1     = EXT_TRIG_IN11 P5_7 J6-2

AOI_OUT = IO0 & IO1

##### Prepare the Demo
1.  Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo

The log below shows the output of the aoi demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
AOI_io_and project.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

When IO0 and IO1 are both high level, the AOI_OUT is high level.
When any of IO is low level, the AOI_OUT is low level.

```

```{container} board-setup
:name: board-frdmmcxa287

##### FRDM-MCXA287

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXA287 board
- Personal Computer

##### Board settings
AOI_OUT = EXT_TRIG_OUT3 P4_5 J6-5
IO0     = EXT_TRIG_IN10 P5_5 J2-15
IO1     = EXT_TRIG_IN11 P5_7 J6-2

AOI_OUT = IO0 & IO1

##### Prepare the Demo
1.  Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo

The log below shows the output of the aoi demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
AOI_io_and project.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

When IO0 and IO1 are both high level, the AOI_OUT is high level.
When any of IO is low level, the AOI_OUT is low level.

```

```{container} board-setup
:name: board-frdmkw43

##### FRDM-KW43

##### Hardware requirements
- Type-C USB cable
- FRDM-KW43 Board
- Personal Computer

##### Board settings
AOI_OUT = EXT_TRIG_OUT3 PTB5 J19-10
IO0     = EXT_TRIG_IN10 PTB4 J19-9
IO1     = EXT_TRIG_IN11 PTA0 J24-1
AOI_OUT = IO0 & IO1

##### Prepare the Demo
1. Connect a USB cable between the host PC and the FRDM board J28.
2. Open a serial terminal on PC for the serial device with these settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3. Download the program to the target board.
4. Either press the reset button on your board or launch the debugger in your IDE to begin running
   the demo.

##### Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
aoi_io_and project.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

When IO0 and IO1 are both high level, the AOI_OUT is high level.
When any of IO is low level, the AOI_OUT is low level.

```

```{container} board-setup
:name: board-frdmmcxw70

##### FRDM-MCXW70

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXW70 Board
- Personal Computer

##### Board settings
AOI_OUT = EXT_TRIG_OUT3 PTB5 J19-10
IO0     = EXT_TRIG_IN10 PTB4 J19-9
IO1     = EXT_TRIG_IN11 PTA0 J24-1
AOI_OUT = IO0 & IO1

##### Prepare the Demo
1. Connect a USB cable between the host PC and the FRDM board J28.
2. Open a serial terminal on PC for the serial device with these settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3. Download the program to the target board.
4. Either press the reset button on your board or launch the debugger in your IDE to begin running
   the demo.

##### Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
aoi_io_and project.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

When IO0 and IO1 are both high level, the AOI_OUT is high level.
When any of IO is low level, the AOI_OUT is low level.

```

```{container} board-setup
:name: board-frdmmcxc353

##### FRDM-MCXC353

##### Hardware requirements
- Type-C USB cable
- FRDM-MCXC353 board
- Personal Computer

##### Board settings
IO0     = XBAR_IN8 (P1_1, J4_2),
IO1     = XBAR_IN7 (P2_17, J2_2/SW3),
AOI_OUT = XBAR_OUT11 (P2_3 LED_GREEN).

AOI_OUT = IO0 & IO1

##### Prepare the Demo
1.  Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

##### Running the demo
When IO0 and IO1 are both high level, the AOI_OUT is high level.
When any of IO is low level, the AOI_OUT is low level.

The following lines are printed to the serial terminal when the demo program is executed.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
aoi_io_and project.

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

```

````