# dsc_cop

## Overview
The COP Example project is to demonstrate usage of the cop driver.In
this example, after 5 times of refreshing in interrupt routine, interrupt will
be disabled, thus the COP is not serviced, then a timeout reset is generated.
Please notice that Write Protect bit in CTRL register are write-once only, it can be cleared only by resetting COP module.
All COP registers are read-only when Write Protect bit set.

## Supported Boards

````{container} board-selector

```{container} board-setup
:name: board-mc56f80000evk

##### MC56F80000-EVK

##### Hardware requirements
- Micro USB cable
- MC56F80000-EVK board
- Personal Computer

##### Board hardware common setting
1. Power setting:
   > Connect J8 pin2 and pin3
   > Connect J6 pin1 and pin2
   > Connect J5 pin1 and pin2
2. Reset pin setting:
   > Connect J11 pin2 and pin3
3. Debugger setting:
   > Connect J13 pin 1-2, 3-4, 5-6, 7-8

##### Board settings
No special settings are required.

##### Prepare the Demo
1.  Connect USB cable between the host PC and the J12 USB port on the target board. It setups Multilink and COM port in PC device manager.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board with Multilink debug configuration.
4.  Launch the debugger in your IDE to begin running the demo.

##### Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
COP example start!

COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
Interrupt disabled, COP will timeout and chip will be reset
Reset due to COP timeout
COP example ends!
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

```

```{container} board-setup
:name: board-mc56f81000evk

##### MC56F81000-EVK

##### Hardware requirements
- 2 x Micro USB cable
- MC56F81000-EVK board
- Personal Computer

##### Board hardware common setting
1. Power setting:
   > Connect J8 pin2 and pin3
   > Connect J5 pin1 and pin2
   > Connect J6 pin1 and pin2
2. Onboard PnE U-MultiLink debugger setting:
   > Connet J11 pin2 and pin3
   > Connect J13 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger PnE U-MultiLink.
     Note: when use external debugger(connected to J10), leave all J13 pins open.

##### Board settings
No special settings are required.

##### Prepare the Demo
1.  Connect USB cable between the host PC and the USB(J26) port on the target board to setup USB to UART bridge.
2.  Connect USB cable between the host PC and the USB(J12) port on the target baord to setup mulitlink debugger.
3.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
4.  Download the program to the target board with PnE U-MultiLink debug configuration.
5.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
    Please be noted default FCF(flash configuration field) makes the MCU boot from flash.

##### Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
COP example start!

COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
Interrupt disabled, COP will timeout and chip will be reset
Reset due to COP timeout
COP example ends!
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

```

```{container} board-setup
:name: board-mc56f83000evk

##### MC56F83000-EVK

##### Hardware requirements
- Micro USB cable
- MC56F83000-EVK board
- Personal Computer

##### Board hardware common setting
1. Power setting:
   > Connect J19 pin2 and pin3
   > Connect J12 pin1 and pin2
   > Connect J13 pin1 and pin2
   > Connect J15 pin1 and pin2
   > Connect J16 pin2 and pin3
   > Connect J17 pin1 and pin2
2. Onboard OSJTAG debugger setting:
   > Leave J5 open
   > Leave J6 open
     Note: J6 is only used(connected) when firmware update for onboard debugger OSJTAG.
   > Connect J11 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG.
     Note: when use external debugger(connected to J10), leave all J11 pins open.

##### Board settings
No special settings are required.

##### Prepare the Demo
1.  Connect USB cable between the host PC and the JM60 USB(J8) port on the target board. It setups OSJTAG and COM port in PC device manager.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board with OSJTAG debug configuration.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. 
    Please be noted that default FCF(flash configuration field) setting makes MCU boot from bootloader. So after reset button press,
    it will wait 5s(wait in bootloader) to run the application code.

##### Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
COP example start!

COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
Interrupt disabled, COP will timeout and chip will be reset
Reset due to COP timeout
COP example ends!
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

```

```{container} board-setup
:name: board-twrmc56f8200

##### TWR-MC56F8200

##### Hardware requirements
- Mini USB cable
- TWR-MC56F8200 board
- Personal Computer

##### Board hardware common setting
1. HW reworkd(workaround):
   > Connect J18(the mini USB port) pin4 and pin5.
     Note: This is due to HW design error, correct setting should be: J18 pin4 left empty and pin5 connected GND.
2. Power setting:
   > Connect J11 pin1 and pin2
   > Connect J6 pin1 and J7 pin2
3. UART setting: 
   > Connect J8 pin3 and pin4
   > Connect J9 pin3 and pin4
4. Onboard OSJTAG debugger setting:
   > Connect J20 pin1 and pin2.
   > Leave J17 open.
     Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG.
   > Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG.
     Note: when use external debugger(connected to J14), leave all J21 pins open

##### Board settings
No special settings are required.

##### Prepare the Demo
1.  Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board with OSJTAG debug configuration.
4.  Launch the debugger in your IDE to begin running the demo.

##### Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
COP example start!

COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
Interrupt disabled, COP will timeout and chip will be reset
Reset due to COP timeout
COP example ends!
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

```

```{container} board-setup
:name: board-twrmc56f8400

##### TWR-MC56F8400

##### Hardware requirements
- Mini USB cable
- TWR-MC56F8400 board
- Personal Computer

##### Board hardware common setting
1. Power setting:
   > Connect J11 pin1 and pin2
   > Connect J6 pin1 and J7 pin2
2. UART setting:
   > Connect J8 pin3 and pin4
   > Connect J9 pin3 and pin4
3. Onboard OSJTAG debugger setting:
   > Connect J20 pin1 and pin2.
   > Leave J17 open.
     Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG.
   > Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG.
     Note: when use external debugger(connected to J14), leave all J21 pins open

##### Board settings
No special settings are required.

##### Prepare the Demo
1.  Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board with OSJTAG debug configuration.
4.  Launch the debugger in your IDE to begin running the demo.

##### Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
COP example start!

COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
COP interrupt is occurred, COP is serviced!
Interrupt disabled, COP will timeout and chip will be reset
Reset due to COP timeout
COP example ends!
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

```

````