# opamp_basic

## Overview

This project shows how to use the OPAMP driver. In this example, the OPAMP works in the internal gain mode,
the positive terminal of the OPAMP is connected to the external input source, and the OPAMP output comes from 2X of the external input voltage.
When the input voltage changes, the OPAMP output changes accordingly.

## Supported Boards

````{container} board-selector

```{container} board-setup
:name: board-mc56f80000evk

##### MC56F80000-EVK

##### Hardware requirements
- Micro USB cable
- MC56F80000-EVK board
- Personal Computer

##### Board hardware common setting
1. Power setting:
   > Connect J8 pin2 and pin3
   > Connect J6 pin1 and pin2
   > Connect J5 pin1 and pin2
2. Reset pin setting:
   > Connect J11 pin2 and pin3
3. Debugger setting:
   > Connect J13 pin 1-2, 3-4, 5-6, 7-8

##### Board settings
Remove jumper for J20, J15, J16.

##### Prepare the Demo
1.  Connect USB cable between the host PC and the J12 USB port on the target board. It setups Multilink and COM port in PC device manager.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board with Multilink debug configuration.
4.  Launch the debugger in your IDE to begin running the demo.

##### Running the demo
Input signal(0-1.65v) to J2-13(feed to GB1, OPAMPB CH0).
Use a multimeter to measure the voltage of TP19, the output voltage is about twice the input voltage.

```

```{container} board-setup
:name: board-mc56f81000evk

##### MC56F81000-EVK

##### Hardware requirements
- 2 x Micro USB cable
- MC56F81000-EVK board
- Personal Computer

##### Board hardware common setting
1. Power setting:
   > Connect J8 pin2 and pin3
   > Connect J5 pin1 and pin2
   > Connect J6 pin1 and pin2
2. Onboard PnE U-MultiLink debugger setting:
   > Connet J11 pin2 and pin3
   > Connect J13 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger PnE U-MultiLink.
     Note: when use external debugger(connected to J10), leave all J13 pins open.

##### Board settings
Remove jumper for J20, J15, J16.

##### Prepare the Demo
1.  Connect USB cable between the host PC and the USB(J26) port on the target board to setup USB to UART bridge.
2.  Connect USB cable between the host PC and the USB(J12) port on the target baord to setup mulitlink debugger.
3.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
4.  Download the program to the target board with PnE U-MultiLink debug configuration.
5.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
    Please be noted default FCF(flash configuration field) makes the MCU boot from flash.

##### Running the demo
Input signal(0-1.65v) to J2-13(feed to GB1, OPAMPB CH0).
Use a multimeter to measure the voltage of TP19, the output voltage is about twice the input voltage.

```

````